Respected Domain Experts,
I have following Specification
Output voltage 30V, Operating frequency is 250kHz, I want bandwidth 30-50kHz.
Can you suggest the best ADC for this applications.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Respected Domain Experts,
I have following Specification
Output voltage 30V, Operating frequency is 250kHz, I want bandwidth 30-50kHz.
Can you suggest the best ADC for this applications.
What type of Digital controller are you using?
Doesn't your digital controller have build in ADCs?
UCD3138 series has 3 EADCs that can be used for your application.
Hello Sir,
I am using FPGA for Digital control of isolated DC-DC Converter for Space Application
I have seen one ADC ADC128S102QML-SP.
Whether its Military Grade Component is available?
I want to check the suitability for Military Grade Applications also
Thanks and regards
Saunak Bhalsod