This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54531: Input Power protection with wide Range input supply

Part Number: TPS54531


Hi team,

I am having wide input supply ranging from 9V to 24V and my device need 5V,4A regulated supply  so I have selected TPS54531.

Basically my application is HMI that will be integrated in a PLC.

Now my concern is about the power input protection(industrial grade) that I need to give to this .

I need at least below mentioned protection

a) Reverse Polarity Protection 

b)Short circuit protection with very fast response.( I have doubt that normal fuses might not respond quickly please suggest)

c)Surge Protection 

d)Over voltage Protection 

can you Please suggest any reference design/document so that I can use it to implement in my design.

I have gone through the eFuses but it doesn't meet my input voltage and output current spec, so I am planning to give the protections using discrete components so that my product is safe from industrial noises.

Since there is some cost constraints I am not going for power module.

Please guide me in this .

Regards,

Karthik