Part Number: TPS7A49
Other Parts Discussed in Thread: LM2674, , TPS7A30, TPS7A39
Hi,
We use the TPS7A4901 and TPS7A3001 in some designs. Are there any plans to have pin compatible devices with a tighter tolerance e.g. 1% instead of the 2.5%?
We often want to increase the supply voltage of OPAMP's to be able to use more range but other devices on the same supply rail have tight maximum supply voltage constraints. So to be able to increase the supply voltage we would need to have a tighter tolerance band around the set point.
Best regards,
Patrick