This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC256301: How to calculate compensation of TLV431 for 40V,3A application

Part Number: UCC256301

Dear Team,

I am working on PFC+ LLC for 40V,3A application for TV application.

The load regulation are pretty worse  if I use EVM default compensation setting.

 The output are 41V at no load but 40V  at 3A load.

Adjust the compensation can reduce the voltage different between different load.

How to optimize the compensation here? Is there any technique document about compensation of UCC25630x?

Thanks 

Shaq