Hi. Pin 30 and 31 is assigned as SYNC-OUT and SYNC-IN in page 8 (pin assignment diagram) but is reversed in page 10 (pin description table). Which is the correct pin assignment? Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
No errata is available for this part in the web site yet.
Any other issues we should know about?
Hi Brad. Can you give some guidance for customers who have existing designs that have tied these pins incorrectly? I believe tha DS suggests pulling up the SYNC-IN pin and leaving the SYNC-OUT pin not connected. With this data sheet mistake, customers have reversed these connections resulting in SYNC-IN being left open. Is this OK? Thanks.
The hardware configuration guide indicates that a pull-up is required on the TDI/SYNC_IN pin under the JTAG Communication and Synchronization section.
This should be clarified, in that, the pull-up is only needed to satisfy the TDI input, however on the UCD9246 both of the TDI and SYNC_IN functions are multiplexed onto the same pin.
For the UCD9248, the TDI and SYNC_IN functions have seperate pins and only the TDI pin needs the pull-up.
Putting an extra pull-up on the SYNC_IN or SYNC_OUT will not interfere with the operation of the device.