This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS26600-02EVM: Current limitation i.e only 2.23A

Part Number: TPS26600-02EVM
Other Parts Discussed in Thread: LM5069

Hi ,

My application require eFuse having following rating

1) Input Voltage 5V to 60V

2) Output voltage 5V to 60V

3) Output Current 8A to 10A

And this TPS26600 has max output current = 2.23A, So please suggest me alternative for this part.

Thanks in Advance!

Prashant