This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Bq34z100-g1: Problems with Learning Cycle

Part Number: BQ34Z100-G1

Hello,

Im using the Bq34z100-G1 with two serial Panasonic LC-RA1212PG (12Ah) Acid Lead batteries (24V).

I run some learning cycles:

1.) Battery is relaxed in any state

2.) Send ENBALE IT

3.) Send RESET

4.) Discharge to empty (2500mA)

5.) Rest for 5h

6.) Charge full with a Mascot Typ2440 (2500 mA)

7.) Rest for 2h

8.) Discharge to empty (2500 mA)

But the learning status never reach 0x05 or 0x06, it always stays 0x04.

ChemID: 803

I use for FC detection the current taper method (change the FC Set % to -1 ).

Attached are the image before and after the Learning cycle. 

I hope you can help me find out what went wrong.

Thank you

DanielLC-RA1212PG Bq34z100-G1.zip