This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54331: Vin UVLO

Part Number: TPS54331

In datasheet page 11, equation between Ren1, Ren2 and Vstart, Vstop is given.

and "VEN is the enable threshold voltage of 1.25 V"

so Ven=1.25V, right?

If that's the case, I would suggest you can just specify it's 1.25V, otherwise it's easy to misinterpret Ven as the voltage on EN pin.