Other Parts Discussed in Thread: TPS62135, TPS62175, LMR33620
Dear e2e support,
Could you help to clarify one point regarding the quiescent current of our LM43602:
- Operating quiescent current (nonswitching) from VIN: should we add the 85µA (under 3.4V) of the I(BIAS-NONSW), to the 5µA typ (under 12Vin), to get the total power consumption of the chip?
- Operating quiescent current (switching): do we have to add anything to the 27µA typ, to get the total quiescent current of the chip?
If i'm right, the 85µA under 3.4Vbias are equivalent to 24µA under 12V, which is quite important. At the end the total quiescent current in non-switching operation would be higher than the one in switching, so I should miss something here ...
Regards,