This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27510-G3: Golden image for bq27510-G3

Part Number: BQ27510-G3

Hi,

 As I am not able to calibrate using external device, can i find golden image for bq27510-G3 so that i can use directly

My battery specification is as below:

Lithium ion battery

Part number: GEB 603463

Voltage: 3.7V

Capacity: 1400mAh

Regards,

Sharmila

  • Sharmilia
    You have to go through the process for creating a golden image. You can not just use any generic chem id.
    The process for generating a golden image is straight forward as i have described in my other post to you. Let me know what portion needs clarification.

    thanks
    Onyx