Other Parts Discussed in Thread: LM10506,
Hello,
The switching waveform seems not PWM even though the mode is changed to force PWM mode.
I would like to share the waveform offline. Would you contact me?
Best regards,
Toshihiro Watanabe
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Watanabe-san,
I ran the same tests on the LM10506 EVM and this time I looked at the SPI pins.
In the attached waveforms, Ch1 = SPI_CS, Ch2 = SPI_DI, Ch3 = B1 output (same net as FB_B1), Ch4 = SPI_CLK. SPI_DO was not needed because there is no data out from the PMIC during a Write command.
When I zoom out and perform the SPI sequence to put B1 into force PWM mode, I can clearly see PFM is exited after the SPI sequence:
When I zoom in and perform the SPI sequence, you can see the voltage of the logic signals (CS, CLK, and DI) exactly as they were transmitted by the MCU.
Although Buck3 Enable, BK3EN, (MSBit) is listed as Read-only, the SPI master on the EVM writes this as a value of 1b.
This is the most obvious difference between the two images, but you can use the above image as a reference for further comparison.
These are Murata multi-layer power inductors.
The closest inductor available in the lab here at TI is the MLP2520V1R5M (TDK 1.5uH multi-layer inductor rated for 1.4A)
I tested the LM10504 EVM with the default VLF3010ST-2R2M1R1 2.2uH inductor, then swapped in the 1.5uH inductor at L1 and saw very little change in Force PWM performance at no load.
The following scope shots were taken with:
Image 1: L1 = 2.2uH Force PWM Off
Image 2: L1 = 2.2uH Force PWM On
Image 3: L1 = 1.5uH Force PWM Off (timescale changed to 1us/div)
Image 4: L1 = 1.5uH Force PWM On
My conclusion is that the value of L1 (1.5uH or 2.2uH) does not impact the functionality of entering Force PWM mode.