Part Number: TPS54240
Hi
my customer has question.
Because there is a possibility of Lost, I would like an answer as soon as possible!
Customer would like to use the external synchronization clock function of the TPS54240.
(Clk=360kHz RT=330kΩ)
It is stated that it is necessary to terminate 50 Ω in the data sheet.
However, with the clock driver currently in use, the Drive capability is insufficient and the clock Level decreases.
Is this 50 Ω mandatory? Is it no problem changing the circuit?
For example, change the part of 330 kΩ + 50 Ω to 165 kΩ + 165 kΩ.
Best Regard
T Kishi