Other Parts Discussed in Thread: BQ20Z80, BQ29312
Hello,
If I put a bq20z80 battery pack into shutdown mode via mfg access command 0x10, are there any cases where the charge & discharge FETs would be turned off when the device wakes back up?
To put into shutdown mode, I'll do the following:
1. Unseal battery
2. Turn OFF FETs by writing 0x0000 to address 0x46
3. Send shutdown command 0x10 to mfg access
This is a bq20z80 pack w/ bq29312 AFE. I've verified the above works and when the pack comes back up, the CHG and DSG FETs are on as desired. Just wondering if there are any conditions that would cause the FETs to not turn on when the device comes out of shutdown mode. E.g., if there's a long enough wait between steps 2 and 3, etc.
Much thanks.