Other Parts Discussed in Thread: LM5118, LM3481
Hello TI Team,
I have following request for a power supply.
Input voltage range of 9..42 V DC.
The output voltage is 12 VDC. Following the requirements of the regulator:
Vin: 9..42 V DC (buck-boost is needed)
Vout: 12 VDC
Iout: 300 mA
Enable Pin
Fsw: > 800 kHz (synchronization with other switching regulator (800 kHz) should be possible)
Soft Start helpful
I selected the LM5002 (datasheet: http://www.ti.com/lit/ds/symlink/lm5002.pdf) because the device looked ok.
Is the LM5002 suitable for this application and can you send me proposal for external components?
If there is a better solution, please let me know.
As this request is a customer request to me; please don't publish the request.
Best regards / Viele Grüße,
Harald
EBV Elektronik