This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
My application has a sensor which requires regulated voltage for precise measurement, also requires it to be low-powered so I need to turn off the sensor when not in use. I have seen that Iq and I shutdown are low for LDO. Can I use it as a load switch as well?
Regards,
Prudhvi Sagar
HI Prudhvi,
As long as VOUT is set higher than VIN, the LDO will operate as a switch. The TPS7A90 is a good choice, I think you may want to look at the TPS7A35 as well.
Regards,
Hello,
If Vout is set higher than Vin LDO will not work right? TO turn OFF the LDO I can directly use EN pin right?
Regards,
Prudhvi Sagar
Hi Prudhvi,
Thank you for confirming that you are using TPS7A90 as an LDO rather than a load switch. You can drive the EN pin of the TPS7A90 with your GPIO. When Ven is logic high, the LDO will regulate the voltage for your sensor. When Ven is logic low, the TPS7A90 will consume 0.1 uA typically (15 uA max) and the output rail will be discharged through the active discharge resistance of 250 Ohm.
Very Respectfully,
Ryan