Part Number: TLV61046A
Hi,
My application is really simple. The DC/DC converter is only used for less than one second to charge a 440uF capacitor @20V.
The input is 2XAAA so minimum voltage around 2.1V. Output 20V. Charging current is limited by a P-chanel Mosfet circuit or a simple power resistor to 200mA.
With 10uH inductor, by applying the equation in the datasheet, I have iL(DC) = 2.27A and iL(P) = 2.34A.
In the datasshet, I don't understand the following reference " Normally, it is advisable to work with an inductor peak-to-peak current of less than 40% of the average inductor current for maximum output current. "
How to choose my inductor regarding my case? Do you have any recommandation? Should I need a saturation of more than 3A? I need a small package in my case because it's for a portable device.
Thank you for your support.