This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TINA/Spice/TPS54331: TPS54331 - Startup issues - Supercapacitor added to the output.

Part Number: TPS54331
Other Parts Discussed in Thread: TINA-TI,

Tool/software: TINA-TI or Spice Models

PROBLEM

Buck converter design was made to operate with minimum input voltage of 5V. However, the lower limit is showing bad results on the startup of the buck converter TPS54331 (datasheet).

OBSERVATIONS

Figure 1 shows part of the schematic with the problematic circuit.

  • Buck converter is not starting when super capacitor is charged. It was observed a relation between super capacitors voltage Supercap and input voltage, when:
    • Supercap voltage 3.50V, buck startup Vin 5.2V.
    • Supercap  voltage 2.90V, buck startup Vin 5.05V.
    • Supercap  voltage 2.50V, buck startup Vin 4.70V.
    • Issue is more likely to happen at 85°C.
      • The board starts at 5.6V when the super capacitors are with 3.22V.

The circuit was simulated with different parameters using TINA Software. However, none of them worked fine, and, the IC is not working with 5V input voltage, it starts the operation at 5.84V on the software.

Using the online tool to select power supply in TI website (WEBENCH) they recommend the use of TPS54331, for this very same application.

 

START UP ONLY

When applied 7V to the input and this voltage is slowly decreased, buck converter keeps operating until the external undervoltage diables the EN pin, at 4.45V.

 

ENABLE PIN

There is a recommendation to use external VIN UVLO to add hysteresis when VIN is lower than Vout + 2V. However, as we are applying 2.8V directly through an inverter port to this pin, the IC is activated.

 

VOUT LIMITATIONS

Since the converter has a limit on minimum and maximum duty cycle. These limit values are calculated and they are within the duty cycle range.

 

RL=35mΩ

VD=0.7V

IOmax=Iomin=3ARds(on)max = 200mΩ

VIN(MIN)=5V

VO(MAX)= 3.85V

 

The Maximum Output Voltage (VO(MAX)) of 3.85V is the higher output voltage that the IC can deliver with a 5V input voltage. So, 3.52V is within the output voltage range and it is ok.

Temperature might cause some variations on these resistance and diode drop, however, the circuit was not tested with this maximum output current (IOmax), but 300mA, which will result in a VO(MAX) of 4.44V.

  • Hello guy,

    schematic looks well.

    can you tell me which cap is super cap? and where is it connected in circuit?

    please upload your waveform.

    best regards

    edwin.

  • The issue is with the Reverse current for the diode. 

    The Diode PN that I'm using has large reverse current compared to others, and the current was flowing back to the IC and somehow the IC wasn't starting up. Perhaps, it is about the BOOT UVLO 2.1V, but not 100% sure of what is going on.

    Changed the diode PN for a diode with 10x lower reverse current and it is working fine the entire temperature range.

    Thanks for the support Edwin.

    Vinicius Marcis.