Other Parts Discussed in Thread: BQ24250, , BQ24040
Maybe this question is more appropriate for the BQ24250 forum?
Is it a recommended practice to add a schottky diode in circuit between the BQ51013B output and BQ24250 input in a wireless battery charging circuit? Or, is this extra part not needed? I am looking at a schottky diode that has approximately 300millivolts Vf at 1A at 25C. I see that the min Vin for the BQ24250 is 4.35V. 5V - 0.3= 4.7V. This is a very small margin, so I wonder if not including the diode is ok.