This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76PL455A: Multidrop Comms Scheme instead of Daisychain

Part Number: BQ76PL455A

Hello,

I am designing a BMS for a battery pack application and I would like to know if the BQ76PL455A is capable of creating such communication scheme. I would like to use for each BQ76PL455A, a microcontroller that controls and communicates with each BQ76PL455A independently. These micros are going to be connected to a CAN bus. I've done the same with the BQ76PL436A and it works perfectly. Would like to know if this can be done with the BQ76PL455A.

Much appreciated,

Carlos Ramos