Hello,
One of my customers is currently use a 100uF 10% tolerance low-ESR ceramic cap on C6 in their application. However, the cap they are using is going obsolete and they only have have options for a 100uF 20% tolerance cap.
Can we get confirmation of what this will effect (if anything)... should this be OK?
The current design: Pin 20 (LL) to 2.2uH 20% tolerance 8A (L1) in series with a 100uF 20% tolerance 6.3V (C6)