I use the MCU sent Passive Balance message :1、 0x91 0x00 0x13 0x08+2 CRC 2、0x91 0x00 0x1f 0x00 +2 CRC 3、 0x92 0x00 0x14 0xff 0xff +2 CRC,toBQ76PL455A-Q1, THE device is not reply. the communication is normal , if the message is wrong ? could you offer some application note about enable Passive balance ,many thanks ~
there some question:1. if i use bq76pl455a monitor Battery 4s ,if the device could work nromal? 2. if there is a battery voltage lower than 1V, is there any affect about balance and the other battery monitor ?