This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM34925: Buck Switch RDS(ON)

Guru 29710 points
Part Number: LM34925
Other Parts Discussed in Thread: LM34926, , LM5018, LM5019

Hi Team,

Is Buck Switch RDS(ON) same between LM34925 and LM34926 under same test condition?
The datasheet shows the value is the same however test condition is different as the following.

- LM34925 (100mA)


-LM34926 (300mA)


Note)
On the other hand, the test condition and value of RDS(ON) are the same between LM5019 (100mA) and LM5018 (300mA).

Best Regards,
Yaita / Japan disty