We're trying to measure backup mode current consumption, and see if it's around 2.25uA as specified. The test procedure is as below.
1. Connect 3.7V at VBAT, and 2.7V at BKBAT.
2. Remove VBAT 3.7V after booting, and only 2.7V BKBAT supplies system
3. Measue drain current from BKBAT ---> 2.7V/7.56uA (100ohm+/-1% resistor as current sense)
4. Re-connect 3.7V at VBAT.
5. Check if RTC keeps when VBAT is removed.
It seems the backup mode current is 7.56uA which is bigger than 2.25uA as specified. Can you help to indicate if there's anything incorrect for our test set-up and configuration?
Thanks,
Antony