This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76PL455EVM: Battery Management - Monitors, Protectors, Authentication and ID Forum

Part Number: BQ76PL455EVM

Hi,

My BQ76PL455EVM was working just fine until yesterday, but now its not waking up, the power led is not lighting and with the GUI I'm getting  "Unable to open com Port" message. 

I have checked with the FTDI settings but it hasn't helped.

The test point voltages are:

VIO  = 5.03V

VDIG = 0V

V5VAO = 4.73V

TX = 4.95V

RX = 5V

TOP = 32.7V 

WAKEUP : 0.144V