This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5116: LM5116 start up issue when SS cap is too large

Part Number: LM5116


Hi, 

I have a startup issue with LM5116 when I put the ss capacitor around 2.2uF. The controller stop switching during the softstart. Please refer to the waveform below: 

The CH3 is the feedback pin voltage and it is lower than the CH4 SS pin, but the control stopped switching. Could you please explain why?

This issue was not observed when I change the ss cap to 0.47uF.

Thank you.

Best Regards,

Oscar