the output of ref3225 is wrong ,the input voltage is 5v(VCC3),but yesterday the output of ref3225 is 2.6v,today the output of ref3225 is2.52v,please help me?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Liufeng28,
The REF3225 is sensitive to startup conditions. This can be seen on pg 9 of the REF3225 datasheet. One solution is to add a RC filter like in the section below.
My recommendation is to use the REF3425. The REF3425 is P2P with the REF3225 and it has improved specifications and does not have input voltage ramp sensitivity.
-Marcoo Z