Part Number: TPS2394
Other Parts Discussed in Thread: TPS2350, TPS23521, LM5067
I have a few questions on TPS2394.
For the design tool which is titled by "slvc064a. TPS2350_DesignCalculator_RevA",
Q1. there is a note - that is "TPS2350/TPS2394 is intended for low power (<250W)".
This power limit comes from where? - FET driving (sink/source current capability) or other viewpoint?
Q2. During the test, I inceased Cramp (controlling the inrush current's slew rate) to 10nF in order to meet to our customer's spec.
Now, the inrush current met to the spec. but I'm afraid that there are some maximum limit to Cramp value.
Are there any side effects if Cramp is increased?
Q3. If TPS2394 is not proper for the application (>250W), pls recommend the other Hot swap controller.
Our spec are Po 1300W, Vin -48Vdc
Thanks
Michael