Other Parts Discussed in Thread: LM5170EVM-BIDIR, , LM5170
Hello!
I meet some issue when debug my LM5170-Q1 board. the schmatic is refer to LM5170EVM-BIDIR, and the Design Calculator . the condition is 50Vin, 12Vout1/50A, 12Vout2/50A.
the DC source is the battery model.
1. I set the OVP point is 17V on the 12Vout, But it can't protect when reach the point.
2. It only can load 1A each channel.