Other Parts Discussed in Thread: TL431
Hi, I'm using TL432B-Q1 in my project. I'm doing worst-case-condition-analysis.
Per TL432BQDBZRQ1 datasheet, it defined many items, eg. reference voltage Vref and deviation of reference voltage over full temperature range VI(dev)...
The system will do calibration at the factory. The operating temperature of the product is -40oC to +125oC. The application is same as Figure 3 in datasheet with R1=1k, R2=3.01k, 5V input.
Which item can be eliminated by doing the calibration?
Which item should be taken into account?