Hello,
I use the LM43601 simple switcher in many designs.
I've selected this component because of its EMC and low current performances.
It works fine when supplied by a 15V source.
When my system goes in standby mode, the LM43601 is supplied by a 5V source. And I need a 5V output which delivers around 300µA.
So I suppose the simple switcher will not switch anymore (will stay closed), and will still be able to drive a current around 300µA with an output voltage around 5V.
But the experiments don't give this theoretical result.
May be there's something wrong in my design, but I'd like to know if my supposition (5V in ~5V out with 300µA load) is correct?
Thank you
Best regards
Alex