This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5165: COT jitter frequency

Part Number: LM5165

I am using LM5165 in COT mode (see schematic snippet image). 

My problem is that the variation in off-time required to regulate the output rail is in a frequency band of interest causing interference with ADCs elsewhere in the system (~25kHz). The switching frequency is varying from ~175kHz to ~200kHz, with RT = 43kOhm (different from schematic snippet).

With RT = 43kOhm, that calculates Fsw of ~530kHz, so I am assuming that my nominal switching frequency is much lower because my load current is not close to maximum, correct?

Is there anything I can do to get the ~25kHz switching noise up above 50kHz or so? I was thinking perhaps a larger inductor will reduce ripple current, causing my nominal load current to be closer to CCM behavior. 

Unfortunately it is difficult to measure the exact load current because I don't have a way to break the +4V rail right at the converter.