Hi,
I'm using TPS61236P in order to convert the typical 2.9/4.1V of a li-ion battery to 5V but, after I designed the pcb circuit (all with >10mil traces), the converter output 5V but less than 200mA and the inductance is making some strange "ticking" noise. I attach the schematic and the board layout I designed based on WEBENCH parameters. Are the traces the problem?
Thank you so much,
Simone