This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2372: TPS2372-4 PoE schematic

Part Number: TPS2372
Other Parts Discussed in Thread: TPS2373-4EVM-758,

Hi,

May I have your support to review TPS2372-4 PoE schematic as attached?

Thanks.

Regards,

Eric

7534.apj80x_POE_2018-03-31_1132.pdf

  • Hi Eric,

    Yes I will take a look at this and get back to you soon. Thanks!
  • Hi Eric,

    A couple of comments regarding the schematic.

    FDMQ8205A is currently no stock on Mouser and Digikey. If you cannot wait and must need a solution sooner, I recommend doing a discrete FET bridge solution like in TPS2373-4EVM-758.
    The dummy load circuit is not needed. The TPS2372 has a feature called "automatic MPS" which is internal to the part and can make the MPS signal automatically if the load is too low. You do have to use the AMPS_CTL in order to implement this feature.

    The DCDC design looks good.

    Thanks!
    Regards,
    Darwin