This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65131EVM-063: change to VIN=5V, VOUT=+/-15V

Guru 20090 points

Part Number: TPS65131EVM-063

Hello,

We would like to use TPS65131EVM on the VIN=5V, VOUT=+/-15V, IOUT=25mA

In this case, can we use TPS65131EVM with the following modification?

C2, C3 : change the 10Vdc rating caps.
Change feedback resistors.

Best Regards,
Ryuji