This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25703A: BQ25703A Pin 18 CELL_BATPRESZ setting

Part Number: BQ25703A

Hi Sir,

The datasheet is show the Pin 18 CELL_BATPRESZ  also sets SYSOVP threshold to 5 V for 1-cell, 

12 V for 2-cell and 18.5 V for 3-cell. 

So Pin18=5V=1Cell, Pin18=12V=2cell , Pin18=18.5V=3cll, CELL_BATPRESZ Absolute Maximum is 7V.

But the EVM is used the VDDA=REGN=6V R20/R21/R24/R28 Partial pressure,

So Pin18=1.2V=1Cell, Pin18=2.72V=2cell, Pin=3.85V=3cell, Pin18=4.22V=4Cell

I am not sure which one is right, May I double confirm with you?

Hugo