This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50-R1: max error 3%

Part Number: BQ40Z50-R1

Hello to TI support team ,

          I have 3S3P cells configuration battery with 0309 ID chem code after finish learning procedure Rdis ='0'  and Qmax updated (changed from init values)  , Update Status 05  .

1. Why my max error value is 3% and  not 1%    ( I did it on 2 batteries  it is the same result , addition cycle do not help )?

2. What is the risk work with max error 3% and not 1% ?

B.R

Alexander Burtakov