Hello,
I have designed a Boost converter with LM3421 according the design guideline provided in the datasheet and it seems to operate well but I get an oscillation when the converter is switched off and I see a strange waveform when dimming. Io is set up to 500mA and the output regulation is quite well adjusted (less or equal 1% at the most).
I attach you the schematic if that can help you to identify better what is going on. (D2 is a Schottky Rectifier with very low forward voltage drop and Main NMOS connected to the gate pin 11, is a Nexfet type).
When the converter switches off, I see an oscillation in the oscilloscope as you can check in the following capture. That means that when I switch off, I see as if the converter would switch on and off for a short period of time and hence that becomes a bit visible when I look at the leds connected to the output. What is happening here? How could I avoid this?
If I zoom the capture, maybe it can be seen more clearly. (Ch2= Io).
I also see some strange captures for output current when I am dimming whatever frequency I use of those that are expected to be used as per my design ( 5KHz, 20KHz). In fact I can see that better, when the difference between the input and the output becomes higher (i.e.: Vinput = 12V and Voutput = 33V). I attach you two captures, the first one is for 12V input, 33V output (11leds) and 20KHz dimming frequency and the second one, is for 18V input, 33V output (11leds) and 20KHz dimming frequency. (Ch1 = Vsw, Ch2 = Io).
When the output current is in "high level", so to speak, it falls down and swings and finally a peak is produced. I am a bit worried about this unexpected peak.
Even though the circuit dimms well and the second capture seems to be normal (I am not completely sure, but I think so), why do I have these oscillations (Vsw) when the transistor is off?. I think that the current peak I get at this moment has relation with this ringing but I do not know what an why I am getting this. When I use the circuit in fixed output current the Vsw waveform is very clean and free of ringing.
Could you please help me with these issues?
Thanking you all in advance.
Regards.