Other Parts Discussed in Thread: BQ76PL536A-Q1
Hello,
I want make BMS with PowerPump Balancing technology ( active cell balancing with multi inductors energy transfers) for automotive application and i'm trying to find the cheapest solution.
I'm using 48 V battery with 36 cells hybrid capacitors (each cell has a 1.4 V)
So, i want to use BQ76PL455A-Q1 as a monitor and a gate driver with his EQn outputs but i doubt if he can driver the mosfet as it is not indicated in the datasheet the maximal voltage for this output(only minimal value
1.8 V mentioned).
if not can i use the BQ76PL536A-Q1 instead of the BQ76PL455A-Q1 as his cell balancing control output can deliever 36 V ?
Thanks in advance.