This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A7002: inputs and output within spec but not able to run in webench

Part Number: TPS7A7002


customer with following requirement

LDO,Vin=6v;Vout=0.5v~2v;Iout=2A

we're looking at the part "TPS7A7002"

however, when i'm trying to run simulations on webench, it failed "says the junction temp too high"

but the input and output V/I are within the range.

please kindly comment if customer can use this part for the requirement

Thanks