Other Parts Discussed in Thread: UCC20520
Hello,
We have been working on making a 3 phase BLDC motor controller with switching implemented through UCC27211 High/Low driver. To start with, we began testing each of the phases of the designed motor controller at no load (nothing connected to the phase outputs). Here is a part of the schematic for reference:
However, after a while IC starts drawing tremendous amount of current (up to 0.4 Amps) through VDD at 12V supply, DC Link at 6V, gets tremendously hot, starts smoking and eventually fails.
Here are some of the scope snapshots for reference:
a. A_BLK - GND
b. HB-HS(Across Cboot)
c. High Side - Channel 1; Low Side - Channel 2
The gate resistances used are 7.5 ohm common for both MOSFET with 1.5 ohm additionally for each parallel MOSFET
Any immediate help towards solving this issue would be highly appreciated. :)