Hello,
I'd like a very long turn on delay. Is it possible to increase the value of CT beyond the suggested 0.01uF in table 1, page 17 of the datasheet? Is there a maximum value? I'm looking for something in the 400ms range, and thus 10uF.
Don
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I'd like a very long turn on delay. Is it possible to increase the value of CT beyond the suggested 0.01uF in table 1, page 17 of the datasheet? Is there a maximum value? I'm looking for something in the 400ms range, and thus 10uF.
Don
Hi Don,
Please see the post below for additional information:
From this post:
"The CT capacitor does not have a maximum value, but exceeding the table limits may cause concern from a thermal perspective depending on the loading conditions. In your application, what is the load capacitance and load current on the output of the TPS22990?"
Thanks,
Alek Kaknevicius