Hi,
BQ40Z50-R1 Load select function have 7 items for user to choice. Does TI has example or data to explain which one is right choice for application?
Constant Current (Load Mode = 0) Constant Power (Load Mode = 1)
0 = Avg I Last Run 0 = Avg P Last Run
1 = Present average discharge current 1 = Present average discharge power
2 = Current() 2 =Current() × Voltage()
3 = AverageCurrent() 3 =AverageCurrent() × average Voltage()
4 = Design Capacity/5 4 =Design Energy/5
5 = AtRate() (mA) 5 =AtRate() (10 mW)
6 = User Rate-mA 6 =User Rate-mW
7 = Max Avg I Last Run (default) 7 =Max Avg P Last Run(default)