This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC2891: use zener Di for VIN at Lo line AC input

Part Number: UCC2891
Other Parts Discussed in Thread: UCC2897A,

Hi all,

I need quickly reply.

PMP6661 circuit  shows  D10  100V zener diode between UCC2897A VIN  and Bridge diode. (AC input 109V to 132V)

www.ti.com/.../slur498.pdf

Can this method be used for UCC2891  (AC input  90V to 138V )?

If yes,  ?? V zener diode, do you recommend?

Best Regards,

H.DOI