This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61120: LDO Maximum Output Current

Part Number: TPS61120


I have a question regarding the maximum output current of the LDO channel when the output voltage is user programmed to 5V.  The datasheet does not show information for VOUT=5V and VIN=3V.  Does this device work with these constraints?  What is the output curve for the conditions I mentioned? I noticed that the graph for output current  LDO @3.3V rolls off quickly and stops between 3V and 3.5V input.  Is this because no data exists or is it a physical limitation of the device?