Other Parts Discussed in Thread: BQSTUDIO, BQ40Z50-R2
I am using the BQ40Z60 battery controller in an intrinsically safe application (IEC60079-11). The design must not under any chip failure mode result in reaching thermal ignition temperatures either of the chip or any associated component. I need to eliminate the amount of power that could be supplied to the chip through the VCC and BAT pins. would 1500 Ohms instead of 10 Ohms cause any issues. the pack is 4 cells. the HIDRV and LODRV FET gates and the PH pins will require protection. is there a problem with series resistance in these lines if i shunt the resistance with capacitors to preserve waveform rise and fall times. I plan to use 50 mA fuses in series with the cell voltage sense lines and balancing resistors.
Please give me your thoughts.
Jerry West