This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS53319: soft start time accuracy

Part Number: TPS53319

Hi,

Could you tell me about soft-start time of TPS53319?
What is the accuracy of 0.7 ms and 1.4 ms?
Please tell me if you have min / max value.
It does not have to be a guaranteed value, so it will be helpful if I can see your opinion.

Best regards,
Yuto Sakai