Hello,
I have a question about D1. D1 is depiced in the datasheet of the BQ76920EVM on page 36.
I have build a batterymanagmentsystem based on the plan of the bq76920evm.
I think there is a short cicuit between J2 the diode D1 and J3, when I connect the battery to the input pins.
What do you think about this thought and why is it nessecary that this diode D1 is placed on this position?
Is D1 a zener-diode?
Thanks for help