Other Parts Discussed in Thread: TPS63050, TPS3839
Hello,
I am having a consumption issue with the TPS82740B.
When the input voltage goes below 2.7V, the current consumption of the IC grows to aproximatly 240 uA.
Measurement conditions:
- The IC is configured to output 3V.
- IC enabled
- CTRL low (load output disabled)
Is this a known issue?
Thanks in advance,
Alejandro