This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP55231: ON/OFF Control

Part Number: LP55231

Hi

My Customer has question.Please cooperate me.

Is it OK for control LED ON / OFF control (05h OUTPUT ON / OFF)?

For example, when D5 is lit up additionally while D1 is lit, it is necessary to write [0001 0001] to [0000 0001], writing 1 again. customer want to check if there is any problem.

Best Regard

T Kishi