Part Number: TPS61029-Q1
I know that "TPS61029-Q1" have two operation mode, Down regulation and Step-Up regulation.
I designed that Vout is 3.3V, so, R3 = 1Mohm, R4 = 180Kohm.
Test condition by Vin
When Vin <= 2.8V, Vout is 3.28V.
When Vin >= 3V, Vout is 2.526V
I understand by page 12 in datasheet , When Vout be designed 3.3V and Vin is more than 2.8V(by Vfb 500mV), change to the down conversion mode.
but, I don't know that why Vout is 2.526V when down conversion mode.
please check.